Skip to main content

Arduino Setup

This section assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-on, please review the following tutorials.

Installing the SparkFun GM-X02B Arduino Library​

This library is built using the SparkFun Toolkit so you'll need to make sure that is installed before using this library. Install the SparkFun Toolkit with the Arduino Library manager by searching "SparkFun Toolkit" and installing the latest version. Users who prefer manually installing Arduino Libraries can download it from the GitHub Repository.

The SparkFun GM-X02B Arduino library works with all nine variants of the GM-XX2B gas sensors on these breakouts. It includes six examples to get users up and running with all sensors. Install Install the library using the Arduino Library Manager tool by searching for "SparkFun GM-X02" and install the latest version. If you'd prefer to manually install the library, you can download it from the GitHub Repository or you can download a ZIP of the repository here.